The SPI data is disconnected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The SPI data is disconnected

1,579件の閲覧回数
Jackson_Ping
Contributor II

Hi,all,

    I had a problem recently,The S32K324 SPI2 clock frequency 10MHz uses DMA to send how the interval between bytes is eliminated.One is the register configuration and the other is the timingiwEcAqNwbmcDAQTRA3UF0QGvBrC3lRJKGI5SVAV-io5SSEkAB9IIsKZwCAAJomltCgAL0gAAiPA.png_720x720q90.jpgiwEcAqNwbmcDAQTRBboF0QIYBrB0DGomrasoVwV-ioO8rMEAB9IIsKZwCAAJomltCgAL0gAA1D0.png_720x720q90.jpg

0 件の賞賛
返信
2 返答(返信)

1,548件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

SPI timing parameters are discussed in chapter 71.3.1.3 of the device RM. So you can refer to it and compare setting with your real signal. It would be great to add generated CS signal as well, to know full frame and a code used to send displayed frame. Could be also a delay is cause by SW overhead.  

BR, Petr

0 件の賞賛
返信

1,515件の閲覧回数
Jackson_Ping
Contributor II

Hi,Petr,

 

Thank you for your answer, I will take some time to study it, thank you.

 

 Best regards,

  Jackson

0 件の賞賛
返信