The GDB Server was not able to establish a connection to the target processor.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The GDB Server was not able to establish a connection to the target processor.

6,598 次查看
xinyu1650
Contributor I

Error in services launch sequence
PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate.

i use my own pcb,

S32 Design Studio for ARM Version: 2018.R1    Build id: 180815

chip:S32K116.

1.png2.png3.png4.png

0 项奖励
回复
6 回复数

4,533 次查看
ajayyadav1996
Contributor III

Adding Kinetis Recovery Tool

0 项奖励
回复

4,533 次查看
ajayyadav1996
Contributor III

Or there is one more possibility that your watchdog is not disabled.

 

Best Regards,

Ajay Yadav

0 项奖励
回复

4,535 次查看
ajayyadav1996
Contributor III

Hello Xinyu and Robin,

 

I was facing same issue and going through comments on software forum, As I am looking into older comments on forum in future someone like me may reach this thread and he might get benefitted from my comment so adding it to this thread.

I found that issue was present with my PE micro hardware (It was faulty), I was able to find root cause with Kinetis Recovery utility tool. 

To download it, Follow below link,
Solved: Can't use PEmicro debugger with S32K118EVB2-Q048 - NXP Community

 

Best Regards,

Ajay Yadav

0 项奖励
回复

6,594 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi xinyu1650,

Have you check the connections and power?

Table 8. S32K1xx - JTAG and SWD interface AN5426.pngPORT G Multilink.png

Have you successfully program the chip before?

Please observe the waveform of the RESET pin with an oscilloscope and upload a picture. If there is a periodic pulse, please let me know the period of the pulse.

Have you tried to using P&E Recovery Utility halt MCU by refer to: https://community.nxp.com/t5/S32K/Can-t-use-PEmicro-debugger-with-S32K118EVB2-Q048/td-p/1376204


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

6,571 次查看
xinyu1650
Contributor I

No change in pin voltage(reset  and vcc  pin),the voltage is 0v.

0 项奖励
回复

6,565 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Would you please power the S32K116?

0 项奖励
回复