Temperature detection function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temperature detection function

1,667 Views
JackChen2022
Contributor I

Hello, I would like to know if the S32K14* series chips have a temperature detection function, or if the entire S32K series has this function, you can also provide reference.

0 Kudos
Reply
3 Replies

1,660 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JackChen2022,

Please refer to: https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,658 Views
JackChen2022
Contributor I

Hi Robin_Shen ,After reading your reply, I understand that the function of the internal temperature sensor may be supported on earlier hardware, and the existing version may be removed? At the same time, some sample programs are not available yet, right?

0 Kudos
Reply

1,653 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

the existing version may be removed? no

some sample programs are not available yet, right? still not sample programs.

0 Kudos
Reply