Temperature detection function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature detection function

1,675件の閲覧回数
JackChen2022
Contributor I

Hello, I would like to know if the S32K14* series chips have a temperature detection function, or if the entire S32K series has this function, you can also provide reference.

0 件の賞賛
返信
3 返答(返信)

1,668件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JackChen2022,

Please refer to: https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,666件の閲覧回数
JackChen2022
Contributor I

Hi Robin_Shen ,After reading your reply, I understand that the function of the internal temperature sensor may be supported on earlier hardware, and the existing version may be removed? At the same time, some sample programs are not available yet, right?

0 件の賞賛
返信

1,661件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

the existing version may be removed? no

some sample programs are not available yet, right? still not sample programs.

0 件の賞賛
返信