TICK duration issue on NXP RTOS using S32K344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TICK duration issue on NXP RTOS using S32K344

2,079 次查看
MVR
Contributor V

Hello all,

I'm trying to define 1ms for each tick using NXP RTOS, but I'm not able to do it.

This is the result:

MVR_0-1709664443686.pngMVR_0-1709664443686.png

Code:

MVR_1-1709664465287.pngMVR_1-1709664465287.png

OsTaskInit AUTOSTART is true.

This is my configuration:

MVR_2-1709664517268.pngMVR_2-1709664517268.png

MVR_3-1709664524950.pngMVR_3-1709664524950.png

I set 1000000 into Period, as we can see this description about the field:

MVR_4-1709664633704.pngMVR_4-1709664633704.png

Also the PIT clock is 40MHz:

MVR_5-1709664657482.pngMVR_5-1709664657482.png

Where am I making a mistake? Can anyone help me please?

Thanks,

MVR

0 项奖励
回复
4 回复数

1,942 次查看
MVR
Contributor V

Anyone, please?

0 项奖励
回复

2,058 次查看
MVR
Contributor V

Hello, anyone can help me, please?

0 项奖励
回复

2,046 次查看
not_a_duck
Contributor III
I noticed that your OsIsr priority is set to 4. is there anything running at a higher priority that could be affecting your period.
Can you increase the priority?
0 项奖励
回复

2,038 次查看
MVR
Contributor V

There is only this timer priority, and also I tried to change to 0 and 60… I got the same result

0 项奖励
回复