Support for FreeRTOS - S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for FreeRTOS - S32K3

Jump to solution
9,539 Views
biju_nair
Contributor III

Hi,

We are building a new platform based on S32K314 part and plan to use FreeRTOS as the OS in this platform. Can someone point me to a location from where i can download the sources ?

Regards, Biju

0 Kudos
Reply
1 Solution
9,523 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @biju_nair 

Enter to the following link: 

S32K3 Microcontrollers for General-Purpose 

VaneB_0-1668534296932.png

There you can find FreeRTOS software for S32K3. If you are not able to see it, please let me know.

 

B.R.

VaneB

 

View solution in original post

8 Replies
9,512 Views
biju_nair
Contributor III

Thanks much VaneB. Appreciate your help.

 

Regards, Biju

0 Kudos
Reply
9,524 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @biju_nair 

Enter to the following link: 

S32K3 Microcontrollers for General-Purpose 

VaneB_0-1668534296932.png

There you can find FreeRTOS software for S32K3. If you are not able to see it, please let me know.

 

B.R.

VaneB

 

6,849 Views
Shashengwan-Yang
Contributor I

Can you give me a link?Thank you

0 Kudos
Reply
9,471 Views
joebarrus
Contributor II

Hi, I'm looking for the same thing and that link doesn't work for me.  See below screen shot.

Is there an updated link?

Thanks,

-Joe

0 Kudos
Reply
9,461 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @joebarrus 

In the link go to the Design Resources -> Software section, there you should be able to find the desired information.

 

B.R.

VaneB

0 Kudos
Reply
9,410 Views
guochuan
Contributor III

Why can't I find the FreeRTOS SDK package based on the K3 platform according to your prompt.

The file name I downloaded is as follows:SW32K3_FreeRTOS_10_4_6_UOS_2_0_1_DS_updatesite_D2209

0 Kudos
Reply
9,376 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @guochuan 

That is the package you need to import to S32DS to have FreeRTOS.

 

B.R.

VaneB

 

0 Kudos
Reply