Strange problems in S32K144W in development (using PE and coding)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Strange problems in S32K144W in development (using PE and coding)

1,387件の閲覧回数
zchy052
Contributor I

Hello expert,

There are strange problems i have met recently.

MCU: S32K144W

IDE version: S32DS V2.2

SDK version: 3.0.0

The project is modified based on the demo project MCSPTE1AK144_PMSM_FOC_2Sh for EVB which applys S32K144.

The problems are:

1. Clock configuration in PE will be recovered itself.

The two places below will always recover itself. While I want to disable them for the usage and S32K144W feature restriction.

 

problem1.PNG

problem1_2.PNG

2. I have developed the bootloader function. A little modification on app will lead to the failure of the running of app although there is no errors reported by S32DS. See pic below.

problem2.png

problem2_2.png

Here buffer is union type, buffer. fltdata.value is float type the same as temp_flt. I don't know why this little modification will cause the failure of software running.

And there may be some other strange modification like this causing the same problem. I think the root cause may be the same.

Can anyone help me on this? Thanks. 

 

 

 

0 件の賞賛
返信
1 返信

1,386件の閲覧回数
zchy052
Contributor I

For problem 2, I have compared the srec files which are used in software update through bootloader, but there are many differences...

タグ(1)
0 件の賞賛
返信