Strange error in Gpt plugin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Strange error in Gpt plugin

741件の閲覧回数
sbadave
Contributor IV

I'm trying to work on S32K3_BJB777A_4.4_R21-11_0.8.0_CD04_D2404 example which has a Phy_665a plugin that I need to work on. For this example, I have installed following (in that sequence):

EB Tresos Studio 29.0.0

SW32K3_RTD_4.4_R21-11_3.0.0

SW32K3_BMS_SDK_4.4_R21-11_1.0.2

SW32K3_BMS_GEN1_SL_SDK_4.4_R21-11_1.0.3_DEMO

S32K3_BJB777A_4.4_R21-11_0.8.0_CD04_D2404

An then copied the required plugins to EB Tresos plugins folder.

After this I added BJB777A example project in EB Tresos and without making any change, just tried Verify and Generate options. During Verify, it threw an error: Invalid XPath expression for attribute "RANGE", pointing to Gpt plugin.

When I checked the required range of GptChannelTickFrequency (0 -> 9223372036854775807), the default value of 8.0E7 is clearly within the range. 

What could be going wrong with the Gpt here ?

MC33665A #MC3377 

sbadave_0-1728564533551.png

 

0 件の賞賛
返信
0 返答(返信)