Spi MCAL initialization error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spi MCAL initialization error

Jump to solution
1,722 Views
psarkar
Contributor III

I am using S32K344 and trying to run the TJA1145a Can Trcv example. I am stuck at Spi_Init() and status remains SPI_UNINIT.image (4).png

I have attached my generate files, any suggestions on how to resolve this will be super helpful. Thanks.

0 Kudos
Reply
1 Solution
1,654 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
Can you specify the version of RTD you're using?
I can only find the example of CanTrcv for S32M276, not S32K344:

cuongnguyenphu_0-1699354272379.pngcuongnguyenphu_0-1699354272379.png


If it possible, please bedug further in Spi_Init function to find out which line is stucked and leads to this issue. Or you can pass me your whole example. 
Your generated seems not so helpful

View solution in original post

0 Kudos
Reply
1 Reply
1,655 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
Can you specify the version of RTD you're using?
I can only find the example of CanTrcv for S32M276, not S32K344:

cuongnguyenphu_0-1699354272379.pngcuongnguyenphu_0-1699354272379.png


If it possible, please bedug further in Spi_Init function to find out which line is stucked and leads to this issue. Or you can pass me your whole example. 
Your generated seems not so helpful

0 Kudos
Reply