Spi MCAL initialization error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Spi MCAL initialization error

跳至解决方案
1,720 次查看
psarkar
Contributor III

I am using S32K344 and trying to run the TJA1145a Can Trcv example. I am stuck at Spi_Init() and status remains SPI_UNINIT.image (4).png

I have attached my generate files, any suggestions on how to resolve this will be super helpful. Thanks.

0 项奖励
回复
1 解答
1,652 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
Can you specify the version of RTD you're using?
I can only find the example of CanTrcv for S32M276, not S32K344:

cuongnguyenphu_0-1699354272379.pngcuongnguyenphu_0-1699354272379.png


If it possible, please bedug further in Spi_Init function to find out which line is stucked and leads to this issue. Or you can pass me your whole example. 
Your generated seems not so helpful

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,653 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
Can you specify the version of RTD you're using?
I can only find the example of CanTrcv for S32M276, not S32K344:

cuongnguyenphu_0-1699354272379.pngcuongnguyenphu_0-1699354272379.png


If it possible, please bedug further in Spi_Init function to find out which line is stucked and leads to this issue. Or you can pass me your whole example. 
Your generated seems not so helpful

0 项奖励
回复