Source & Sink Current for S32K324

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source & Sink Current for S32K324

1,276 Views
hemanths
Contributor III

Hi NXP Team,

What is the maximum current that can sink to a GPIO pin/ maximum current that the GPIO pin can source in S32K3xx microcontrollers?

0 Kudos
Reply
1 Reply

1,262 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @hemanths,

The higher the current the bigger the voltage drop from VDD/VSS.

The datasheet specifies the min. guaranteed current at  

VOL <= 0.7V

VOH >= VDD_HV_A/B - 0.7V

for all the GPIO types.

danielmartynek_0-1708512129865.png

 

Refer to the IBIS model of the device for more information.

 

Best regards,

Daniel

0 Kudos
Reply