Some Questions about SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some Questions about SRAM

Jump to solution
2,064 Views
Embedded_novice
Contributor III

I want to know why SRAM is divided into SRAM_ L and SRAM_ H. What is the difference between these two? What are they applicable to respectively? furthermore I found SRAM_ H and SRAM_ The addresses between L are discontinuous, why do we do this?

Thank!

0 Kudos
Reply
1 Solution
2,041 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It offers certain advantage for performance optimization.

SRAM_L offers single-cycle access for core code bus whilst SRAM_U offers single-cycle access for core system bus. Other accesses are backdoor and these take two clocks.

However SRAM address space is continuous, because SRAM_L extends downwards and SRAM_U extends upwards as you can see on the picture below:

davidtosenovjan_0-1706276924845.pngdavidtosenovjan_0-1706276924845.png

 

 

View solution in original post

0 Kudos
Reply
2 Replies
2,042 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It offers certain advantage for performance optimization.

SRAM_L offers single-cycle access for core code bus whilst SRAM_U offers single-cycle access for core system bus. Other accesses are backdoor and these take two clocks.

However SRAM address space is continuous, because SRAM_L extends downwards and SRAM_U extends upwards as you can see on the picture below:

davidtosenovjan_0-1706276924845.pngdavidtosenovjan_0-1706276924845.png

 

 

0 Kudos
Reply
2,025 Views
Embedded_novice
Contributor III
Thank you very much for your answer!
0 Kudos
Reply