Some Questions about SRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some Questions about SRAM

ソリューションへジャンプ
2,096件の閲覧回数
Embedded_novice
Contributor III

I want to know why SRAM is divided into SRAM_ L and SRAM_ H. What is the difference between these two? What are they applicable to respectively? furthermore I found SRAM_ H and SRAM_ The addresses between L are discontinuous, why do we do this?

Thank!

0 件の賞賛
返信
1 解決策
2,073件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It offers certain advantage for performance optimization.

SRAM_L offers single-cycle access for core code bus whilst SRAM_U offers single-cycle access for core system bus. Other accesses are backdoor and these take two clocks.

However SRAM address space is continuous, because SRAM_L extends downwards and SRAM_U extends upwards as you can see on the picture below:

davidtosenovjan_0-1706276924845.pngdavidtosenovjan_0-1706276924845.png

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,074件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It offers certain advantage for performance optimization.

SRAM_L offers single-cycle access for core code bus whilst SRAM_U offers single-cycle access for core system bus. Other accesses are backdoor and these take two clocks.

However SRAM address space is continuous, because SRAM_L extends downwards and SRAM_U extends upwards as you can see on the picture below:

davidtosenovjan_0-1706276924845.pngdavidtosenovjan_0-1706276924845.png

 

 

0 件の賞賛
返信
2,057件の閲覧回数
Embedded_novice
Contributor III
Thank you very much for your answer!
0 件の賞賛
返信