Setup and Hold time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setup and Hold time

1,387 Views
kamalakannan_go
Contributor I
Hello NXP Team,
   we are using the S32K uC interface with various slaves. every slave has different setup and hold time requirements,
Do you have any standard calculations / Methods to ensure the slaves setup and hold time meet the uC requirement, we will not face any issues even worst case scenario?   

SETUP AND HOLD TIME.PNG

0 Kudos
Reply
1 Reply

1,325 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello [email protected],

Unfortunately, there is no more information available.

The characteristics ware taken at the conditions specified in the datasheet 6.3.2 QuadSPI AC specifications.

And the min values of the input signal should be met.

Regards,

Daniel

0 Kudos
Reply