[Security] about Memory Management

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Security] about Memory Management

ソリューションへジャンプ
2,516件の閲覧回数
Gideon
Contributor III

Architecture: FreeRTOS 10.2.1 with S32K144

Our security has the following requirement:
"Do not grant unnecessary processes or tasks the permission to read or write to memory regions through process boundaries or MMU."

Q1: Does the S32K144 support process boundaries or MMU mechanisms?
Q2: If yes, what is the setting to enable process boundaries or MMU?

0 件の賞賛
返信
1 解決策
2,398件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Gideon,

As I mentioned, the MCU has an MPU only.

FreeRTOS has MPU support for the ARM MPU.

However, the CM4 core on S32K144 does not have ARM MPU, there is NXP MPU on the bus instead.

You would need to implement it on your own. There is SDK MPU driver though.

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,494件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Gideon,

Unfortunately, the S32K1xx series do not have MMU.

MSCM_CPxCFG3 = 0x101.

MSCM_CPxCFG3[MMU] = 0.

The S32K1xx HW supports:

  • The system MPU prevents access of different bus masters to address ranges. It is typically intended for use by the safety application to prevent non-safety related modules access to the application's safety-relevant resources.
  • The peripheral bridge can restrict read and write access to individual I/O modules based on the origin of the access and its state (user mode/supervisor mode).
  • Register protection prevents individual registers from any manipulation until the registers are unlocked.

 

Regards,

Daniel

0 件の賞賛
返信
2,439件の閲覧回数
Gideon
Contributor III

the S32K1xx series do not have MMU ==> OK, I understand.
But does the S32K144 series with FreeRTOS 10.2.1 support Process boundary mechanisms?

0 件の賞賛
返信
2,399件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Gideon,

As I mentioned, the MCU has an MPU only.

FreeRTOS has MPU support for the ARM MPU.

However, the CM4 core on S32K144 does not have ARM MPU, there is NXP MPU on the bus instead.

You would need to implement it on your own. There is SDK MPU driver though.

 

Regards,

Daniel

0 件の賞賛
返信