[Security] CSEC components's Encryption and decryption performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Security] CSEC components's Encryption and decryption performance

1,867 Views
Gideon
Contributor III

Dear NXPs:

From UseNote:AN5401 We  know :

1.Setup: M4 Core running at 80 MHz and Flash running at 26.67 MHz.  

2.measured to process 112bytes of data

According to the above two conditions, the encryption and decryption performance of AES-128-CBC is as follows:

ENC_CBC: Execution Time =  0.028718;

DEC_CBC: Execution Time = 0.029153;

Q:We design S32K146's M4 Core running at 64 MHz and Flash running at 16 MHz.measured to process 112bytes of data, what is the performance of ENC_CBC and DEC_CBC?

 

 

 

 

 

0 Kudos
Reply
3 Replies

1,852 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Gideon 

I'm afraid that we do not have numbers for all possible use-cases. If some specific performance numbers are required, our recommendation is to measure it directly in your system. Easiest option is to toggle a GPIO before and after calling of a function and measure the time by an oscilloscope.

Regards,

Lukas

0 Kudos
Reply

1,845 Views
Gideon
Contributor III

Dear NXPs:

       Is there any theoretical estimation formula or empirical formula on NXP?

0 Kudos
Reply

1,820 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Sorry, there's no such formula.

Regards,

Lukas

0 Kudos
Reply