Secure_Boot_for_S32K324

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure_Boot_for_S32K324

1,195件の閲覧回数
Ranjith_kumar
Contributor II

Hi,

I'm  trying to do Hardware secure engine(HSE) in S32k324 controller and I'm using S32 DS Platform 3.5  with RTD version 3.0.7.  

First, i  created new project and i was trying to configure HSE module but it is not working and it is troughing lots of errors. Also i  was Tried to find example project, but it is not available in that RTD Version. 

So could you please share any example project for HSE in S32K324 Controller? and let me if you need anything from my end.

 

 

 

Regards,

Ranjith_Kumar 

0 件の賞賛
返信
1 返信

1,149件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ranjith_kumar 

In RTD version 3.0.0 P07, the available example codes that uses HSE are Crypto_CmacCtr_KeyGenBD_S32K344, Crypto_SymmetricPrimitives_S32K344, and Hse_Ip_AesEncAsyncIrq_S32K344. 

Additionally, example codes are available without RTD that provide different use case scenarios to show the capabilities of the HSE FW on different devices. 

S32K3 Standard Software > Automotive SW - S32K3 - HSE Firmware

S32K3 MCUs for General Purpose HSE Demo Examples

 

BR, VaneB

0 件の賞賛
返信