Secure_Boot_for_S32K324

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure_Boot_for_S32K324

1,196 Views
Ranjith_kumar
Contributor II

Hi,

I'm  trying to do Hardware secure engine(HSE) in S32k324 controller and I'm using S32 DS Platform 3.5  with RTD version 3.0.7.  

First, i  created new project and i was trying to configure HSE module but it is not working and it is troughing lots of errors. Also i  was Tried to find example project, but it is not available in that RTD Version. 

So could you please share any example project for HSE in S32K324 Controller? and let me if you need anything from my end.

 

 

 

Regards,

Ranjith_Kumar 

0 Kudos
Reply
1 Reply

1,150 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ranjith_kumar 

In RTD version 3.0.0 P07, the available example codes that uses HSE are Crypto_CmacCtr_KeyGenBD_S32K344, Crypto_SymmetricPrimitives_S32K344, and Hse_Ip_AesEncAsyncIrq_S32K344. 

Additionally, example codes are available without RTD that provide different use case scenarios to show the capabilities of the HSE FW on different devices. 

S32K3 Standard Software > Automotive SW - S32K3 - HSE Firmware

S32K3 MCUs for General Purpose HSE Demo Examples

 

BR, VaneB

0 Kudos
Reply