Sample code for interfacing four MC33774 with S32K312 Microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample code for interfacing four MC33774 with S32K312 Microcontroller

1,478件の閲覧回数
amattanchery
Contributor I

In our new project we have a hardware configuration with S32K312 controller interfaces to MC33664 and then TPL communication will be connected to four MC33774. 

To quick start the project, would like to check if there is any application note or source code available to interface between  S32K312 -> MC33664 -> MC33774

0 件の賞賛
返信
1 返信

1,468件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @amattanchery 

The available information about the MC33774/MC33664 with S32K3 is related to Battery Management Unit solutions, which is under NDA (Non-Disclosure Agreement) the information is not public, and we can not share the information due to the security levels when working with an automotive part such as this. Contact your NXP representative for further support in this part.

 

B.R.

VaneB

0 件の賞賛
返信