SWT Expires Only 8 Times

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWT Expires Only 8 Times

Jump to solution
3,509 Views
vgonzalez
Contributor II

Hello. I have a SWT configured as shown in the image below. When I service the SWT, it works as expected. Wen I purposely don't refresh the SWT to prove that it can reset the software execution, it does reset, but only 8 times in a row. After 8 times, it doesn't reset any more and the microcontroller seems not to be running any code. When I have used a SWT with other microcontrollers, the SWT keeps resetting indefinitely if it is not refreshed.

I am not running in debug mode.

Board: S32K3x4EVB-Q257

vgonzalez_0-1668091948487.pngvgonzalez_0-1668091948487.png

Thanks in advance!

Tags (1)
0 Kudos
Reply
1 Solution
3,403 Views
vgonzalez
Contributor II

For anyone having this issue, it is related to the value of FRET (section 32.8.7 of the Reference Manual). By changing the value of FRET on boot as shown below, the SWT doesn't have a limited number of times to reset the system.

#define MC_RGM 0x4028C000

#define MC_RGM_FRET MC_RGM+0x18 

char *pFRET = (char *)MC_RGM_FRET;

*pFRET = 0;

View solution in original post

3 Replies
3,404 Views
vgonzalez
Contributor II

For anyone having this issue, it is related to the value of FRET (section 32.8.7 of the Reference Manual). By changing the value of FRET on boot as shown below, the SWT doesn't have a limited number of times to reset the system.

#define MC_RGM 0x4028C000

#define MC_RGM_FRET MC_RGM+0x18 

char *pFRET = (char *)MC_RGM_FRET;

*pFRET = 0;

3,480 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @vgonzalez 

According to the information provided, I suggest you to try testing just the SWT without the intervention of any other module, the section 65.3.8 Test SWT operation of the S32K3xx Reference Manual, Rev. 5 shows how to ensure that the internal countdown timer is working properly.

Also, take a look at Swt_Ip_Example_S32K344, the examples use SWT timeout interrupt to feed itself. Each 1 second, the SWT timeout expired and the SWT interrupt will reset the counter by writing the service sequence. SWT will be de-initialized after performing 5 times SWT service.

Let me know if it is helpful for you.

 

B.R.

VaneB

0 Kudos
Reply
3,436 Views
vgonzalez
Contributor II

Thank you for your reply @VaneB 

I ran the sample code Swt_Ip_Example_S32K344 and it worked as you described. The example is configured with Operation Mode as Interrupt. As described in the reference manual, this mode generates an interrupt on an initial time-out, and a reset on a second consecutive time-out. To allow the reset to occur, I removed the SWT de-initialization after performing 5 times SWT service and the reset occurred only 8 time as originally described. Is it possible that this is how NXP designed the SWT to operate?

0 Kudos
Reply