SWD problem on s32k144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWD problem on s32k144

ソリューションへジャンプ
2,910件の閲覧回数
lohrsistemas
Contributor IV

I have successfully programmed my device but now I cannot connect with MCU.

I use SWD interface. It can be the case that I use SWD pins as output and in my code I set PTA4 and PTA5 as output. Can it be the case?

What can I do?
タグ(2)
0 件の賞賛
返信
1 解決策
2,665件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It seems to be the case.

It was discussed in this thread: https://community.nxp.com/message/987643 

You can use the PEmicro recovery utility mentioned in the thread.

Regards,

Daniel

元の投稿で解決策を見る

2 返答(返信)
2,666件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It seems to be the case.

It was discussed in this thread: https://community.nxp.com/message/987643 

You can use the PEmicro recovery utility mentioned in the thread.

Regards,

Daniel

2,665件の閲覧回数
lohrsistemas
Contributor IV

Hi Daniel,
I did not have the hardware PE micro, so I tried with the SEGGER.
Trying several times to reset the power of my board, had a moment when I was able to program it.

Okay, that saved my board. However I will go through this problem if I have to use these pins in a project where the pins of the MCU are completely used, and the last resort is to share the SWD pins. I suggest having some commentary on the datasheet of this item, guiding the risks of using SWD pins for general purposes.

0 件の賞賛
返信