SPI Max Length for S32k148

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Max Length for S32k148

1,483 次查看
rohit_alate
Contributor II

Hello Community,

I want to interface the GPU with NXP S32k148 Board via SPI for my application, so I am having Que like how much max distance i.e Cable length it will cover with max speed? with NXPs LPSPI component if I configured.

Thanks in advance,
Rohit

0 项奖励
回复
1 回复

1,470 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Rohit,

The LPSPI module is specified at the below conditions, so the max. load on the line is 50pF.

danielmartynek_0-1631622272951.png

 

Regards,

Daniel

0 项奖励
回复