SPI Max Length for S32k148

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Max Length for S32k148

1,486件の閲覧回数
rohit_alate
Contributor II

Hello Community,

I want to interface the GPU with NXP S32k148 Board via SPI for my application, so I am having Que like how much max distance i.e Cable length it will cover with max speed? with NXPs LPSPI component if I configured.

Thanks in advance,
Rohit

0 件の賞賛
返信
1 返信

1,473件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Rohit,

The LPSPI module is specified at the below conditions, so the max. load on the line is 50pF.

danielmartynek_0-1631622272951.png

 

Regards,

Daniel

0 件の賞賛
返信