SPI Communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Communication

1,521件の閲覧回数
saurabh_sharma
Contributor I

I'm interfacing a thermocuple-to-digital converter operating at 3.3V to a MCU-S32K148 operating at 5V.

This converter is communicating via SPI. My  concern is whether communication at 3.3V level will be successfully accomplished or I need to add signal conditioning network in between?

0 件の賞賛
返信
1 返信

1,383件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

S32K148 dev-kit works on 3.3V and on 5V. pastedImage_1.png

If you must keep S32k148 power supply to 5V and external device to 3.3V I recommend you to use level shifters because threshold for HIGH is 3.25V if you power the S32K148 to 5V.

pastedImage_2.png

Best regards,

Razvan

0 件の賞賛
返信