SDK Attachment Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK Attachment Issue

1,602 Views
prabtani
Contributor I

I am trying to create an example application project for LED blinking for S32K358. When creating a project, I am not able to attach the SDK and it shows the error that "SDK cannot be attached as it does not support the toolchain required by the project".

I have installed S32DS 3.6.4. Have installed SDK "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip"Error_1.png

0 Kudos
Reply
3 Replies

1,579 Views
prabtani
Contributor I

Hello Robin,

Thank you for your response. Could you please send the link to the latest RTD that will be supported with 3.6.4 S32DS IDE. 

Also in your step 3, I do not see any SDK to attach. It shows empty list.

0 Kudos
Reply

1,575 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Click S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -> S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0
By the way, the latest S32K3 RTD 6.0.0 was tested in S32 Design Studio 3.6.1. I have not tried to install S32K3 RTD 6.0.0 in S32DSv3.6.4.

0 Kudos
Reply

1,581 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

1. I don't recommend installing an older version like "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip."
2. Is there any special reason for needing such an old RTD version? Otherwise, I recommend installing the latest version, "SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite.zip."
3. Go to File -> New -> S32DS Application Project, select S32K358, and then click ... to choose the SDKs. I recommend selecting it at that time.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply