SBC_FS26_example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SBC_FS26_example

1,402件の閲覧回数
Albatros
Contributor III

Hello,

I am using SBC_FS26_example and FS26 in my board works in normal mode. However when i try to write something to any registers with Sbc_fs26_WriteRegister(boolean bIsFailSafe, uint8 u8Address, uint16 u16WriteData) function it does not write it. I try to read it with Sbc_fs26_ReadRegister(boolean bIsFailSafe, uint8 u8Address, Sbc_fs26_RxFrameType* pRxData) and i see that i can not write it. What could be the problem?

タグ(2)
0 件の賞賛
返信
1 返信

1,352件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Albatros,

I hope all is great with you. Thank you for using the NXP communities.

Could you please share more information about the sample code used? I mean, what is the source code?

What are the registers that you are trying to modify?

Do you mean that you cannot write it or read it?

Regards,

David

0 件の賞賛
返信