SAE J2602 version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAE J2602 version

3,482 Views
abpaz
Contributor I

Hi,

I am using S32 Design Studio for Arm V2.2. Do you know which revision of SAE J2602 it is compatible with? Can I update any component to generate a LIN driver to be compliant with the latest revision of SAE J2602 (202110)?

Thanks a lot.

0 Kudos
Reply
5 Replies

3,475 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @abpaz 

Can you tell us the MCU that you are using? And also, which software (SDK or RTD)?

0 Kudos
Reply

3,461 Views
abpaz
Contributor I

Hi @VaneB,

Thanks for your fast answer.

I am using S32k118 uC and the SDK: S32SDK_S32K1xx_RTM_4.0.1.

Thanks a lot!

0 Kudos
Reply

3,449 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @abpaz 

J2602 protocol is LIN 2.0 based. It contains LIN 2.0's modules to support Signal management, network management, scheduler and J2602 status management. The goal of J2602 is to improve the interoperability and interchangeability of LIN devices within a network by resolving those LIN2.0 requirements that are ambiguous, conflicting, or optional. Moreover, J2602 provides additional requirements that are not present in LIN2.0. For example: fault tolerant, operation, network topology, etc. Different to LIN2.1 protocol, J2602 does not support sporadic and event trigger frames in communication.

 

B.R.

VaneB

0 Kudos
Reply

3,439 Views
abpaz
Contributor I

Hi @VaneB,

Yes, but I need to know which revision of SAE J2602 is implemented in the SDK that I mentioned before and if and how I could generate a LIN driver compliant with the latest revision of this protocol.

B.R.

Thank you!

0 Kudos
Reply

3,431 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @abpaz 

The LIN projects included in the SDK are just an emulation of LIN over UART. If you want to work directly with LIN, look at Automotive SW - S32K1 - LIN Stacks.

VaneB_0-1674683612723.pngVaneB_0-1674683612723.png

Note: SAE J2602/1 LIN Network for Vehicle Application, September 2005.

 

0 Kudos
Reply