SAE J2602 version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAE J2602 version

3,483件の閲覧回数
abpaz
Contributor I

Hi,

I am using S32 Design Studio for Arm V2.2. Do you know which revision of SAE J2602 it is compatible with? Can I update any component to generate a LIN driver to be compliant with the latest revision of SAE J2602 (202110)?

Thanks a lot.

0 件の賞賛
返信
5 返答(返信)

3,476件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @abpaz 

Can you tell us the MCU that you are using? And also, which software (SDK or RTD)?

0 件の賞賛
返信

3,462件の閲覧回数
abpaz
Contributor I

Hi @VaneB,

Thanks for your fast answer.

I am using S32k118 uC and the SDK: S32SDK_S32K1xx_RTM_4.0.1.

Thanks a lot!

0 件の賞賛
返信

3,450件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @abpaz 

J2602 protocol is LIN 2.0 based. It contains LIN 2.0's modules to support Signal management, network management, scheduler and J2602 status management. The goal of J2602 is to improve the interoperability and interchangeability of LIN devices within a network by resolving those LIN2.0 requirements that are ambiguous, conflicting, or optional. Moreover, J2602 provides additional requirements that are not present in LIN2.0. For example: fault tolerant, operation, network topology, etc. Different to LIN2.1 protocol, J2602 does not support sporadic and event trigger frames in communication.

 

B.R.

VaneB

0 件の賞賛
返信

3,440件の閲覧回数
abpaz
Contributor I

Hi @VaneB,

Yes, but I need to know which revision of SAE J2602 is implemented in the SDK that I mentioned before and if and how I could generate a LIN driver compliant with the latest revision of this protocol.

B.R.

Thank you!

0 件の賞賛
返信

3,432件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @abpaz 

The LIN projects included in the SDK are just an emulation of LIN over UART. If you want to work directly with LIN, look at Automotive SW - S32K1 - LIN Stacks.

VaneB_0-1674683612723.pngVaneB_0-1674683612723.png

Note: SAE J2602/1 LIN Network for Vehicle Application, September 2005.

 

0 件の賞賛
返信