S32k358 IPCF references or training support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k358 IPCF references or training support

1,240 Views
soumik1506
Contributor III

Hello experts, I am trying to use the IPCF middle ware to exchange message between core 0 and core 7 of my s32k358 board. I am running the IPCF example project and i am it is always going to a hard fault. I did not make any changes to the example.

Next, i made a copy of this example and kept only 1 un managed channel in the Core 0 project and kept the configurations for the core2 as it is. This this i am getting Hard Fault error at the state of the un manged channel.

I am not able to understand the configurations that were set in the example. I am trying to , but i am getting stuck. If there is a reference manual or training material, please share it, it will make things easier

Tags (2)
0 Kudos
Reply
1 Reply

1,211 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It seems on my side, example works normally when I keeps all Software dependencies defined in SW32K3_IPCF_4.1.0_D2312_ReleaseNotes.pdf.

Please, try to set up optimization level to None (-O0).

0 Kudos
Reply