S32k344 development board debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k344 development board debugging

Jump to solution
2,746 Views
dashe
Contributor II

Hello,everyone.

Can s32k344 development board be debugged with ULINK debugger?

0 Kudos
Reply
1 Solution
2,737 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi dashe,

s32k344 development board can be debugged with Keil's ULINK debugger.(So I think ULINK2 is also ok) But it is recommended that you submit a technical service request for ARM confirmation.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

2 Replies
2,741 Views
dashe
Contributor II

Can s32k344 development board be debugged with ulink2 debugger?

0 Kudos
Reply
2,738 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi dashe,

s32k344 development board can be debugged with Keil's ULINK debugger.(So I think ULINK2 is also ok) But it is recommended that you submit a technical service request for ARM confirmation.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------