S32k314 Timer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k314 Timer

1,712件の閲覧回数
dpsdprtmvl
Contributor II

Dear All,

Hello, I using S32k314 board (RTD3.0.0), but i have a question about STM in GPT module.

 

According to S32k3xx RM.pdf,  I found S32k314 allowed 2 instances of STM, STM_0 and STM_1 .

dpsdprtmvl_0-1742085963865.png

But, S32k314 don't have a clock about STM_1 in example code at design studio 3.5 version.

 

I wonder "S32K314 also supports STM_1, but why is there no clock configuration for STM_1 in the example code?"

 

Thanks.

 

0 件の賞賛
返信
3 返答(返信)

1,610件の閲覧回数
dpsdprtmvl
Contributor II

Thank you for your reply.

 

I tested adding the STM1 module, but the S32k314 board doesn’t boot properly when it runs GPT Init.


After looking into it, I found out that the S32K314 doesn’t actually have a clock for STM1.

 

As a result, after removing STM1,  the S32k314 board boot normally,


It operation doesn’t match what’s described in the S32k3xx reference manual.

0 件の賞賛
返信

1,601件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Ok, but once you configure clock you also have to enable it to the peripheral.

Did you enabled it in ME module for STM0 and 1?

It is in MCU plugin:

petervlna_0-1745393794182.png

I have tested it here and everything is running as expected:

petervlna_1-1745393824869.png

 

Attached is the example file if you like to test it

Best regards,

Peter

0 件の賞賛
返信

1,681件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Example code usually implement only basic demo features to show the functionality.

I wonder "S32K314 also supports STM_1, but why is there no clock configuration for STM_1 in the example code?"

I have just open the example for GPT and simply added STM0 and 1 modules and everything works as expected. Both are supported.

petervlna_0-1744792924522.png

petervlna_1-1744792939153.png

Simply follow the example or screenshot above and add STM1.

Best regards,

Peter

0 件の賞賛
返信