S32k314 STM Clock question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k314 STM Clock question

470 Views
dpsdprtmvl
Contributor I

We are currently migrating from the S32K344 environment to the S32K314.

During the GPT initialization process, a core power-down occurs.

One of the key differences we've identified between the S32K344 and the S32K314 is the generation of the STM1_CLK (STMB_CLK).
In the case of the S32K344, STMB_CLK is properly generated.

In the S32K314 environment, we forcibly added the STMB_CLK configuration to the generated Clock_Ip_PBcfg.c file.
After doing so, the GPT initialization worked correctly and the system booted without any issues.

However, we don’t understand why simply adding this configuration would cause the GPT init to work as expected.
We are trying to understand how this change alone resolves the issue.

Tags (1)
0 Kudos
Reply
1 Reply

442 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If it is a new project, it is recommended to use the latest S32K3 RTD, because many bugs are fixed.

Have you tested the latest S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 5.0.0?

Best Regards,
Robin

0 Kudos
Reply