S32k1Xx FlexIO timer 16-bit counter mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32k1Xx FlexIO timer 16-bit counter mode

跳至解决方案
1,934 次查看
yuegao1996
Contributor II

Hi, 

   when i read S32k1 user manual, about flexio timer 16bit counter mode, it says " In 16-bit counter mode, the full 16-bits of the counter and compare register are used to configure either the baud rate of the shift clock or the shifter bit count." 

   dose it mean that the 16bit counter is FFFF at the beginning, and the timer cmp register is used for shifter bit count ?

many thanks.

0 项奖励
回复
1 解答
1,919 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

    16-bit timers control the loading, shifting and storing of the shift registers, the counters load the contents of the compare register and decrement down to zero on the FlexIO clock.

 

BR!

     Jim.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,920 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

    16-bit timers control the loading, shifting and storing of the shift registers, the counters load the contents of the compare register and decrement down to zero on the FlexIO clock.

 

BR!

     Jim.

0 项奖励
回复
1,918 次查看
yuegao1996
Contributor II

Thanks !

0 项奖励
回复