S32k148EVB_Q176 MCU replacement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k148EVB_Q176 MCU replacement

661 次查看
RainXX
Contributor I

Hi,dear

    I was bought a board of S32k148EVB_Q176,but My error of operation causes MCU to be very hot and high, when normal power supply.So,I bought another MCU(S32k148HAMLU) replace the bad MCU(S32k148UJALU) .When I was download and debug firstly that was normal with OpenSDA,At second times the MCU can't enter download and debug functional.Maybe startup address was error?If I buy a some MCU(S32k148UJALU) to replace,that have the same of question?

So,I have a question that need bootloader application code before download and debug of firstly?

 

标记 (1)
0 项奖励
回复
2 回复数

650 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

S32k148HAMLU
H: 80 MHz
A: CAN FD, FlexIO, Security

S32k148UJALU
U: 112 MHz (Not valid with M temperature/125C)
J: Ethernet, Serial Audio Interface, CAN FD, FlexIO, Security (S32K148 only)

If your program does not include Ethernet, Serial Audio Interface, it may be caused by clock configuration. If you use the example where the system clock is not initialized, can you debug successfully? For example: AN5413SW\S32K1xx_cookbook\Examples\S32K148_Project\S32K148_Project_hello


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 项奖励
回复

644 次查看
RainXX
Contributor I

Hi,dear

I can't debug use the example where the system clock is not initialized successfully.It always error.

Like follow picture 

1.png

0 项奖励
回复