S32k148 - Firmware update methods

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k148 - Firmware update methods

3,484 次查看
sathish_sekar
Contributor III

I am working on firmware update methods for s32k148.

I  have seen a/b swap firmware update mechanism in https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/s32-autom...

for s32k146.

i.e Referring the application note https://www.nxp.com/docs/en/application-note/AN12323.pdf.

It contains information for s32k144/146.

I looking the same for s32k148. 

Is this already available in nxp forum or I should create  for myself??

Could anyone provide details for firmware updates in s32k148(evb)?

标签 (1)
0 项奖励
回复
3 回复数

2,859 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Sathish,

there's version only for S32K144 and S32K146. It's supposed to be sample code only, so if you need to port it to S32K148, it's necessary to do that by yourself. S32K148 is superset of S32K146, so it should be quite easy to port it.

If you need just simple bootloader (no A/B swap), there's also AN12218:

https://www.nxp.com/docs/en/application-note/AN12218.pdf 

https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip 

Regards,

Lukas

0 项奖励
回复

2,859 次查看
laplk
Contributor I

Hello Lukas,

Source code to build file .bin (blink led) any special things? It is built by S32Ds or other IDE?

If you have this source, please send to me.

Thanks and Regards

Akai

0 项奖励
回复

2,859 次查看
sathish_sekar
Contributor III

Hello Lukas,

Thanks for the response.

Porting the project form s32k146(https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip)  to s32k148 is the  best option, and current i am trying this.

Thanks an Regards

Sathish

0 项奖励
回复