S32k146 UART RX interrupt not receiving entire buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k146 UART RX interrupt not receiving entire buffer

1,126件の閲覧回数
bhanu_p
Contributor I

Hi,

i'm using S32k146 custom board PCB  in that i'm trying to get the RX buffer using interrupt method but the thing is my interrupt  call back function not triggering to get entire buffer.

for Example : if i send "AT+RESET" to MCU  my call back function only triggering 3 times and i'm getting buffer only "AT" remaining buffer i'm not getting and my call back event is showing as "UART_EVENT_ERROR" 

please go through the below given code for your reference

uart_init(void)
{
	LPUART_DRV_Init(INST_LPUART1, &lpuart1_State, &lpuart1_InitConfig0);
	LPUART_DRV_InstallRxCallback(INST_LPUART1, iot_rx_callback, NULL);
        LPUART_DRV_SendDataBlocking(INST_LPUART1, ser_tx_cmd0, 4U, 100);
}

void iot_rx_callback(void *driverState, uart_event_t event, void *userData)
{
	(void) driverState;
	(void) userData;

    if (event == UART_EVENT_RX_FULL)
    {
        if ((buffer[bufferIdx - 1] != '\r') && (buffer[bufferIdx] != '\n') && (bufferIdx != (BUFFER_SIZE - 1U)))
        {
            bufferIdx++;
            LPUART_DRV_SetRxBuffer(INST_LPUART1, &buffer[bufferIdx++], 1U);
        }
        else
        {
	  bufferIdx=0;
           rx_complete = true;
        }
    }
}

while(1){

	int ret =LPUART_DRV_ReceiveData(INST_LPUART1, buffer, 1U);
	if(ret=STATUS_SUCCESS){
	while(LPUART_DRV_GetReceiveStatus(INST_LPUART1, &bytesRemaining) == STATUS_BUSY);
	  ser_buffer_index=0;
	}
/*********/
own code
/********/

}

 

Screenshot 2024-10-14 173728.png

my normal TX data is transmitting properly without any trouble  only problem i'm facing in RX  data 

 

0 件の賞賛
返信
1 返信

1,089件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I recommend you to refer to the example in S32K1xx Lpuart IDLE detected with DMA transfer.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信