S32k146 Process expert- No active project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32k146 Process expert- No active project

跳至解决方案
2,272 次查看
PU1
Contributor II

The  pop up window comes, when I try to generate code . 

I'm am using DS32 ARM 2.2 

pop when try to generate codepop when try to generate code

Also not able to add module to projectwhen try to add module no option is not enablewhen try to add module no option is not enable

0 项奖励
回复
1 解答
2,133 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that your project is baremetal without SDK included. Please refer to the Attaching an SDK to an existing project of S32DS_ARM_User_Guide.pdf.

Attaching an SDK to an existing project.pngAttaching an SDK to an existing project.png

Please select the SDKs next time you create a new project.

Select SDK.pngSelect SDK.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,115 次查看
PU1
Contributor II

Thanks for your reply  @Robin_Shen,

i was following same procedure.

my issue is solved. ,,some packages are not added.

0 项奖励
回复
2,134 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that your project is baremetal without SDK included. Please refer to the Attaching an SDK to an existing project of S32DS_ARM_User_Guide.pdf.

Attaching an SDK to an existing project.pngAttaching an SDK to an existing project.png

Please select the SDKs next time you create a new project.

Select SDK.pngSelect SDK.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------