S32k144 CSEC error state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k144 CSEC error state

Jump to solution
1,817 Views
fan1234
Contributor III

Hi, team:

     from AN5401 , i know the error is reported in the “Error Bits” field when any error occurring during the CSEC command execution, and i want to confirm what's the impact with the chip? 

     for example, if i update a key without increase the counter value, the error bit will be "CSEC_KEY_UPDATE_ERROR", then the key will be unavailable or what, and will it affect the use of flash modules?

 

Thanks in Advance

Cor

Tags (1)
0 Kudos
Reply
1 Solution
1,777 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @fan1234 

if you get "CSEC_KEY_UPDATE_ERROR", nothing will happen. The  original key can be still used, it's just not updated because you provided wrong data. It does not affect flash modules.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
2 Replies
1,778 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @fan1234 

if you get "CSEC_KEY_UPDATE_ERROR", nothing will happen. The  original key can be still used, it's just not updated because you provided wrong data. It does not affect flash modules.

Regards,

Lukas

0 Kudos
Reply
1,762 Views
fan1234
Contributor III
other error bits will be the same? will any error of csec affect flash modules or original kes?
0 Kudos
Reply