S32k144 CAN FD Setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k144 CAN FD Setting

2,138 Views
woolim
Contributor II

I am currently using the S32k144 MCU, and we are using the CAN FD setting in that MCU as follows.

woolim_0-1747184107036.png

According to that, I'm trying to match the setting below using 40 MHz Clock.
Arbitration Phase: 500kbps / 80% sampling
Data Phase: 1Mbps / 80% sampling

I'm trying to match the CAN setting with other MCUs more accurately to the TQ, but the value of segment is automatically set, so how can I change it?

Additionally,  according to the above setting value, it is calculated as Arbitration Phase TQ: 17, what setting do I need to do to change the TQ to 80?

 

 

 

0 Kudos
Reply
3 Replies

2,109 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@woolim

1.1. Uncheck the option below, and you can configure the parameters yourself

Senlent_0-1747193633128.png

2.The link provides a calculation excel for calculating CAN parameter configuration.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-LPCxxxx-CAN-CAN-FD-bit-timing-cal...

 

0 Kudos
Reply

2,060 Views
woolim
Contributor II

This is CAN FD communication that I have previously set up.

woolim_0-1747805117880.png

And it is the setup of CAN FD communication that I will change.

woolim_1-1747805160581.png

 

Both settings have the same Bitrate and Sampling Point, but each parameter is different. If I set it to the previously set value, will it be compensated separately?

When setting the bitrate with the previously set values, I would like to ask you because it seems that the bitrate does not come out.

 

 

0 Kudos
Reply

2,051 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@woolim

"will it be compensated separately?"

To be honest, I don't understand what you mean

If you are not sure about your configuration, you can check the generated file to see what parameters you actually configured

0 Kudos
Reply