S32k118 Debugging and CAN Transmission Error Inquiry

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k118 Debugging and CAN Transmission Error Inquiry

997 Views
Juns
Contributor I

hello, 

I'm a newbie studying about s32k.

I am facing two inquiries. Please refer to the information below

 

1. When conducting CAN communication using the FLEXCAN component, an error such as a photo occurs in the Vector. Please let me know what to do about this part.

Juns_0-1731551403481.png

Juns_2-1731551551499.png

Juns_3-1731551564869.png

I want to use SPI and SBC to do CAN communication, what should I do?

 

 

2. During debugging, if I click the debugging Resum button by writing the expressions value with the variable name as shown in the picture below, an error occurs, how do I handle it?

Juns_1-1731551529855.png

 

 

 

0 Kudos
Reply
1 Reply

956 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) se sure board is powered by 12V so SBC and its CAN transceiver is active. Also be sure SBC is in Forced Normal Mode operation (default mode). If not must be configured via SPI, or put back to default mode.

2) Expression window does not show variables if code is running, once you stop code variables are updated.

BR, Petr

0 Kudos
Reply