S32k Design Studio 3.4 version Example project Import Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k Design Studio 3.4 version Example project Import Problem

2,681 Views
Lisha
Contributor III

Hi Team,

I am importing example project of Multicore_singleElf So I tried to download the RTD package(SW32K3_RTD_4.4_2.0.3) and update the Extension. But, I am getting this Error. Please help me on this.

Looking forward for your response.

Lisha_0-1743482691468.png

 

BR,

Lisha

 

0 Kudos
Reply
6 Replies

2,648 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Lisha

Make sure your S32 DS V3.4 is clean.

I try to install this version from begining.

1. Offline Install V3.4 Update 3 as i said before

Senlent_0-1743494152657.png

2.Install RTD 2.0.3

Senlent_1-1743494839556.png

then you should able see RTD 2.0.3 in "Available/Update"

then install it(you can see i have success to installed.)

Senlent_2-1743495007333.png

 

 

 

0 Kudos
Reply

2,667 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Lisa

I don't know if you followed the requirements. According to the release note, you need to install "S32 Design Studio for S32 Platform v.3.4 Update 3" first.

Senlent_0-1743488165072.png

 

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=13216587

Senlent_1-1743488371178.png

 

0 Kudos
Reply

2,661 Views
Lisha
Contributor III

Ok Thank You

 

BR,

Lisha

0 Kudos
Reply

2,654 Views
Lisha
Contributor III

Hi Team,

 

Now this was showing, Could you please help us how to resolve this?

Lisha_0-1743492898366.png

 

BR,

Lisha

 

0 Kudos
Reply

2,624 Views
Lisha
Contributor III

Hi Team,

I installed all the requirements but I got the error Message only. Following method I followed,

1. Installed the S32 DS V3.4 (V3.4 update 3 window installer is not available )

2. Installing the New SW SW32K3_S32DS_3.4.3_D2112 in S32 DS.zip

3. Installing the New SW SW32K3_RTD_4.4_2.0.3_DS_updatesite_D2302.Zip

After that I update the SW Extension but It shows 

Lisha_0-1743738816081.png

 

Anyone Please help us, It is urgent to import the Project of Multicore Single Elf Example but This Error got me tricky.

BR,

Lisha

 

0 Kudos
Reply

2,592 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Lisha

Please show me screenshots of each of your installation steps, because I have tried to install it from scratch and followed the steps in my previous reply to you, and I did not encounter such a problem.

0 Kudos
Reply