S32K3xx RTD 7.00 examples missing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx RTD 7.00 examples missing?

2,695 Views
Henrik-Wires
Contributor IV

Just upgraded S32K396 RTD package from 6.0.0 to 7.0.0 I notice that it seems there is no examples included in this version of the RTD?

Are the examples found somewhere else now?

S32K3 S32DS-ARM AUTOMOTIVE-RTD 

6 Replies

2,652 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Henrik-Wires 

We understand your concerns.

As stated in the software release notes, no example code is currently available. However, we were informed that a release planned for February 2026 is expected to include example code.

Please note that this is a tentative date and may be subject to change.

 

BR, VaneB

0 Kudos
Reply

2,603 Views
Henrik-Wires
Contributor IV
A quick feedback on that decision is that not including the examples, even if not qualified for the release is a major issue. The quality of the documentation heavily relies on the examples being available. Not having the examples in an release is a complete show stopper for people to get up and running on the platform.
So in future releases please do include examples even if not verified. With that same note in the release notes.

2,560 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Henrik-Wires 

Thank you for your feedback. We apologize for the inconvenience.

0 Kudos
Reply

2,665 Views
Henrik-Wires
Contributor IV

I see now that the release notes mention that "Driver examples are not supported in this release", which I guess means the release is without examples. And with DS only supporting one version installed at a time this causes a bit of headache.

0 Kudos
Reply

2,579 Views
FelixR
Contributor III
I had the same headache as you. I decided to install the 7.0.0 SDK Version on my main installation of the s32ds and make a separate installation directory for the old 4.0.0 version just to take the example projects as reference.
0 Kudos
Reply

2,563 Views
Henrik-Wires
Contributor IV
6.0.0 also includes the examples.
0 Kudos
Reply