S32K3xx OTA BootLoader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx OTA BootLoader

3,487 Views
Alicetian
Contributor I

Hello:

I learned that the S32K3xx has OTA capabilities,When the OTA feature is enabled,Supports A/B swap and OTA Roll back.

Traditional firmware updates are via BootLoader,As shown in the following figure.

Boot.png

If I want to use the S32K3xx OTA function,Do I still need a separate BootLoader? Or integrate BootLoader flashing into App Firmware.

If a separate BootLoader is required,How the BootLoader memory region is divided.

Looking forward to your reply,Thanks!

0 Kudos
Reply
3 Replies

3,473 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Alicetian 

There is an OTA demo for S32K3 that you can find at S32K3 Reference Software -> Automotive SW - S32K3 Reference Software,

If you are not able to access it, please get in touch with your NXP representative for access.

Also, take a look at Automotive Security and Over-the-Air (OTA) solution with S32K3 MCU.

 

B.R.

VaneB

0 Kudos
Reply

3,411 Views
Alicetian
Contributor I

Hello,

Thank you very much for your reply, Whether there is a firmware installation project, For example S32K3x4_HSE_FW_INSTALL_Demo,So I can install the AB Swap Firmware Through PE tool.

0 Kudos
Reply

3,397 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Alicetian 

You can download HSE FW and HSE demo app from S32K3 Standard Software -> S32K3 Reference Software packages.

0 Kudos
Reply