[S32K3XX] C40_Ip using for accessing Code flash memory patition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32K3XX] C40_Ip using for accessing Code flash memory patition

ソリューションへジャンプ
1,521件の閲覧回数
Changhawn
Contributor III

Hi.

I am developing flash access using C40_Ip api in bootloader.

Data memory partition(0x10000000) can be accessed by that API.

But code memory partition(0x500000 ~ 0x007FE000) can not be accessed.

Hard fault assert is happened. 

C40_Ip API is located in SRAM like below.

Changhawn_0-1721353208571.png

Could you give me some guide or hint for this debugging?

Thank you in advance.

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,501件の閲覧回数
Changhawn
Contributor III

Basic working is confirmed.

My access region is not wrong.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,502件の閲覧回数
Changhawn
Contributor III

Basic working is confirmed.

My access region is not wrong.

0 件の賞賛
返信
1,495件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Changhawn

Is your problem solved?

I see that you have already set your answer as a solution.

0 件の賞賛
返信
1,492件の閲覧回数
Changhawn
Contributor III
Yes.
It's work normally
0 件の賞賛
返信
121件の閲覧回数
NXP开发者
Contributor II

I encountered the same problem as you. When writing to the PFLASH, a hardware fault occurred. Could you please tell me how you solved it?

タグ(1)
0 件の賞賛
返信