S32K3X8EVB-Q289 (k358 device) Sample Driver code for QSPI module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3X8EVB-Q289 (k358 device) Sample Driver code for QSPI module

3,052件の閲覧回数
Ragul
Contributor I

Hi, I am using S32K3X8EVB-Q289 (k358 device) and I am not finding any example codes for this device. I need to implement QSPI for External FLash(S26KL512S) kindly do the needful ASAP. Sample driver code would be helpful.  S32K3X8EVB-Q289 

0 件の賞賛
返信
3 返答(返信)

2,980件の閲覧回数
Ragul
Contributor I

Thanks for your support. In description of that code, it is stated that the code is applicable for XS32K3X8CVB-Q289 PCB 53108 RevX3 SCH RevA1 board. I need example for S32K3X8EVB-Q289. And can you clarify on which external flash memory it is configured on the code?? MX25L6433F or S26KL512S ?? since S26KL512S external flash chip is present in S32K3X8EVB-Q289 board.

0 件の賞賛
返信

2,963件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ragul,

The same memory is used between the two boards (S26KL512S), so you should be able to use this same example as reference without problems.

Best regards,
Julián 

0 件の賞賛
返信

2,992件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ragul,

There is an example code for the Hyper Flash memory used on S32K3X8EVB-Q289 in RTD 3.0.0. Below is the path, but I will still attach it to my reply.
"C:\NXP\SW32K3_RTD_4.4_R21-11_3.0.0\eclipse\plugins\Mem_43_ExFls_TS_T40D34M30I0R0\examples\S32DS\S32K358\Qspi_Ip_Example_S32K358"

Best regards,
Julián

0 件の賞賛
返信