S32K385 board support and examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K385 board support and examples

跳至解决方案
2,389 次查看
Rob_t
Contributor I

Hello NXP community! I apologise if this any has been asked before but I would like to know a few things about the s32k358. I am using the S32K3X8EVB-Q289 evaluation board.

-Is there IAR support for this chip/board?

-Is there J-Link support for this chip/board?

-Is there a specific sdk/bsp for this board?

So far I have found that the answer to all these questions is no, but I would like to confirm, please. Moreover I am missing the example projects in s32ds 3.5 relating to the k358. I am using the latest version of the development package as well.

Please let me know if you have any information on these matters and any further suggestions. Thank you!

0 项奖励
回复
1 解答
2,353 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Rob_t 

Firstly I think that did you mean S32K358.

Is there IAR support for this chip/board? IAR offers broad NXP coverage with support for Kinetis, LPC, Vybrid, i.MX and S32K, as well as S08.

Is there J-Link support for this chip/board? J-Link offers support to S32K3 devices, specifically the ones listed in the below link. 

Supported Devices - J-Link - NXP - S32K3

Is there a specific SDK/BSP for this board? The available software that supports S32K358 is the S32K3 Real-Time Drivers Version 3.0.0 (released on March 31) and onwards. You can download it from S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M.

As the S32K358 is still not a mass-market device, not all the information is public. I suggest you contact your NXP representative for further information on this part.

Note: the first two questions are generalized for the S32K3, because of the reason previously mentioned.

 

B.R.

VaneB

在原帖中查看解决方案

1 回复
2,354 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Rob_t 

Firstly I think that did you mean S32K358.

Is there IAR support for this chip/board? IAR offers broad NXP coverage with support for Kinetis, LPC, Vybrid, i.MX and S32K, as well as S08.

Is there J-Link support for this chip/board? J-Link offers support to S32K3 devices, specifically the ones listed in the below link. 

Supported Devices - J-Link - NXP - S32K3

Is there a specific SDK/BSP for this board? The available software that supports S32K358 is the S32K3 Real-Time Drivers Version 3.0.0 (released on March 31) and onwards. You can download it from S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M.

As the S32K358 is still not a mass-market device, not all the information is public. I suggest you contact your NXP representative for further information on this part.

Note: the first two questions are generalized for the S32K3, because of the reason previously mentioned.

 

B.R.

VaneB