S32K358 SBC_FS26 module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K358 SBC_FS26 module

7,527 Views
ALXY_WANG1
Contributor II

If you migrate Sbc_fs26_example_Ip_S32K388 sample file to S32K358 project file, and directly call the wake-up API function and mode jump API function based on the sample file, but the corresponding setting mode is not entered after the software is executed during the debugging process, do you need to set other parameters to correctly call the mode jump function?

0 Kudos
Reply
7 Replies

7,478 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Alxy,

please try to use a software for the FS26 SBC from our HVBMS bundle attached. It is for the S32K358. Please let me know if it is suitable for your. If not, I will contact an application team for advice on how to fix the issue with your migrated code.

With Best Regards,
Jozef

0 Kudos
Reply

7,406 Views
ALXY_WANG1
Contributor II

After porting, when the source code is automatically generated by the SBC and SPI module peripherals, an error message is directly displayed, indicating that the spi. h folder is not available

0 Kudos
Reply

7,364 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Alxy,

thank you for additional details. I guess the missing spi.h folder is missing in the example from the HVBMS? Let's please return to the previous issue. Please check if the FS26 has switched to STANDBY mode by checking if the relevant regulators are on and other off as suggested by an software engineer below.

DESCRIPTION

According to their software implementation, I cannot see any verification point after the call of Sbc_fs26_SetOperatingMode(SBC_FS26_OPMODE_STANDBY)

After entering Standby mode, some regulators on FS26 will be OFF, you can suggest them to check.

JozefKozon_0-1715229298479.png

 

With Best Regards,
Jozef

0 Kudos
Reply

7,414 Views
ALXY_WANG1
Contributor II

示例文件为 S2K344 文件。我可以直接将 FS26 模块移植到文件 358 中并确保所有相关配置相同吗

0 Kudos
Reply

7,454 Views
ALXY_WANG1
Contributor II
This file is still an S32K344 sample file. Can S32K358 be directly ported and burned to S32K3X8EVB-Q289HWUM for debugging? Currently, the S32K344 file cannot be burned to S32K3X4EVB-Q257_HW-UM
0 Kudos
Reply

7,464 Views
ALXY_WANG1
Contributor II
Which SDK version of the S32DS that corresponds to the installation of this sample file can be provided
0 Kudos
Reply

7,443 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Alxy,

I have download the sample file from this link. There is plenty of other software for the S32x family. It might be interesting for you. Please note, that you need to be registered on the NXP page to be able to open it.

JozefKozon_0-1715078510260.png

Meanwhile, I will contact an application team for an advice on your question.

"If you migrate Sbc_fs26_example_Ip_S32K388 sample file to S32K358 project file, and directly call the wake-up API function and mode jump API function based on the sample file, but the corresponding setting mode is not entered after the software is executed during the debugging process, do you need to set other parameters to correctly call the mode jump function?"

With Best Regards,
Jozef

0 Kudos
Reply