S32K358 RGMII Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K358 RGMII Interface

6,942件の閲覧回数
VNeve
Contributor I

I am looking to interface 1Gbps Ethernet PHY to S32K358 through RGMII. 

On searching for pins to map for the interface I found that in IO signal table only 2 Tx and 2 Rx pin options are available while 4 Tx and 4 Rx pins are required to complete the interfacing. Other available Tx and Rx pins shows for "(MII Mode Only)" and possibly can't be use as RGMII interface. Is there any application note or reference schematic available?

I have read the communication on forum but not found any conclusive answers.

Please help here. Thanks!!

タグ(2)
0 件の賞賛
返信
2 返答(返信)

6,798件の閲覧回数
Dinesh_Guleria
NXP Employee
NXP Employee

GMAC of S32K358 support the RGMII for 1000 Mbits/sec.

 

Please refer the Schematic in design file in this link. You can use the same pins for RGMII :--

https://www.nxp.com/design/design-center/development-boards-and-designs/S32K3X8EVB-Q289

 

Also refer the excel sheet in the attachment of the reference Manual, for GMAC pin details.

0 件の賞賛
返信

6,793件の閲覧回数
Dinesh_Guleria
NXP Employee
NXP Employee

GMAC of S32K358 support the RGMII for 1000 Mbits/sec.

 

Please refer the Schematic in design file in this link. You can use the same pins for RGMII :--

https://www.nxp.com/design/design-center/development-boards-and-designs/S32K3X8EVB-Q289

 

Also refer the excel sheet in the attachment of the reference Manual, for GMAC pin details.

0 件の賞賛
返信