S32K358 LockStep Core1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K358 LockStep Core1

跳至解决方案
1,346 次查看
darknite2023
Contributor III

Hi.

I am using a S32K3X8EVB-Q289 devkit board and have a question regarding lockstep (which is enabled):

  • Lockstep core0's PRTN0_CORE0_STAT register shows that its clock is active.
  • Lockstep core1's PRTN0_CORE1_STAT register shows that its clock is inactive.

Just wondering if the lockstep's 2nd core needs to be explicitly configured to run i.e. enable its clock? Or, the fact that lockstep is enabled,  the contents of locktstep core1's PRTN0_CORE1_STAT register is not valid?

Thanks in advance.

 

0 项奖励
回复
1 解答
1,259 次查看
bryan_brauchler
NXP Employee
NXP Employee

Hello,

 

When configured for lockstep, the cores will be configured to run in lockstep before being released from reset. Hence the Core1 registers have no effect.

 

Best,

 

Bryan

在原帖中查看解决方案

2 回复数
1,260 次查看
bryan_brauchler
NXP Employee
NXP Employee

Hello,

 

When configured for lockstep, the cores will be configured to run in lockstep before being released from reset. Hence the Core1 registers have no effect.

 

Best,

 

Bryan

1,249 次查看
darknite2023
Contributor III
Hi Bryan. Thanks for the response and clarifying my doubt. As a suggestion, it would be nice to state this in the PRTN section of the S32K3XX RM.
0 项奖励
回复