S32K358 IO port voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K358 IO port voltage

221 Views
Chenxu1
Contributor I

Hi,I met  a strange problem:
The schematic diagram of the K358 is as follows,

If I remove the magnetic bead, then the IO port output is 5V, if the magnetic bead is welded on, it is 5.48V.  Using magnetic beads with different parameters, it is also 5.48V
expecting a reply

Chenxu1_0-1721970067279.png

Chenxu1_1-1721970082954.png

 

 

0 Kudos
Reply
1 Reply

200 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Chenxu1,

Can you share a complete schematic of the board in a better quality?

If you don't want to share it here, create a ticket.

I see two L12 and L11 there, which one do you mean?

I understand there is 5.48V towards the ground, but where do you measure it?

Where exactly do you measure the 0.48V potential, can you mark it in the schematic?

 

Thank you,

Daniel

0 Kudos
Reply